TGML Common Attributes
The following attributes are applicable to all TGML elements:
Attribute | Type | Description |
---|---|---|
ID |
String |
The identity of the element. Reserved for scripts and other entities that need to use unique element identifiers to access specific elements. |
Name |
String |
The name of the element. The primary use is to identify exposed elements such as Bind. |